DUG_IR Controller 1Module-00

Resetting the device

You can reset the device to factory default manually.
Press the reset button 14 times in 10 s using the pin.
The LED stays in red for 10 s.
NOTE: After reset, the device is ready for pairing.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.