DUG_IR Controller 1Module-00

Changing the brightness report frequency

You can change the brightness report frequency using the Wiser app.
To change the brightness report frequency:
  1. On the Devices page, tap Devices.
  2. Select the IR Controller to change the location.
  3. On the top-right corner of the screen, tap Settings.
    The Hub Settings page appears.
  4. Enter the new value in the Brightness Report Frequency field.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.