DUG_IR Controller 1Module-00

Changing the temperature report frequency

You can change the temperature report frequency using the Wiser app.
To change the temperature report frequency:
  1. On the Devices page, tap Devices.
  2. Select the IR Controller to change the location.
  3. On the top-right corner of the screen, tap Settings.
    The Hub Settings page appears.
  4. Tap Temperature Report Frequency.
  5. Select the desired value from the following list:
    • 1 deg

    • 2 deg

    • 3 deg

    • 4 deg

    • 5 deg

    NOTE: The minimum temperature value is 1 deg and the maximum value is 5 deg.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.