DUG_IR Controller 1Module-00

LED indication

Pairing

User Action

LED Indication

Status

Press the reset button 4 times in 10 s.

Blinking red rapidly.

Pairing mode is active for 3 minutes. When pairing is completed, the LED will display a solid red.

Press the push-button 8 times in 10 s to change the Wi-Fi access point mode.

Blinking red rapidly.

The device is ready to connect with the new Wi-Fi access point.

Resetting

User Action

LED Indication

Status

Press the reset button 14 times in 10 s.

Solid blue and red (pink).

The device is in reset mode. It is reset to the factory settings.

LED Indicator Mode

LED Indicator Mode

LED Indication

Paired but not connected to Wi-Fi (Router disconnected)

LED blinks red per second

Connected to cloud

Solid green

Connected to Wi-Fi but no cloud connection (No internet)

LED blinks green per second

OTA update

LED blinks red and green alternatively

Reset state / Not paired / Not added

Solid red

Key pairing mode

Solid red for 15 seconds

Key controlling

LED blinks red per second

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.