DUG_IR Controller 1Module-00

Changing the device region

You can change the device region using the Wiser app.
To change the device region:
  1. On the Devices page, tap Devices.
  2. Select the IR Controller to change the location.
  3. On the top-right corner of the screen, tap Settings.
    The Hub Settings page appears.
  4. Tap Select Region.
  5. Select the desired region from the following list:
    • ASIA

    • US

    • EU

    • JAPAN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.