Create and Manipulate Markups
After selecting the appropriate operational map, In the
upper right corner of the app, tap the Markups button.
This operational map has five types of markup assignment available to select.
After placing a markup, you can edit, remove, cancel, and close/reopen it. In some circumstances, you can also rename markup jobs in the Job Panel.
Your markup toolbar might look similar to the following:
- To draw freehand in the map, tap the Freehand
tool, then draw in the map as desired. When you tap the down arrow to the right of the tool, you can select from four different types of lines in three different colors.
- To place a callout in the map, tap the Callout
tool, then tap once in the map to place the callout. A simple text box activates along with the keyboard.
- To place a dimension line in the map, tap the Dimension
Line
tool. Tap once in the map and a grey dot is placed at the starting point.
- To highlight an area of the map, tap the Highlight
tool. Tap once to place the first vertex, then tap to place more vertices.
- To place a point in the map, tap the Point
tool, then tap spots in the map where you want points placed. When you tap the arrow under the tool, you can select from three different types of points.
- To place a line in the map, tap the Line
tool. Tap to place vertices, then tap the Finish Edit
button.
- To place a polygon in the map, tap the Polygon
tool, then keep tapping until you have the shape you want. Tap the Finish Edit
button to complete the polygon.
- To edit a markup, tap the Edit
tool.
- To edit a callout, tap on it to activate the text box, then make your edits. Or if you want to move the callout, tap the Move directional arrows then tap the new location in the map.
- To edit a point, tap on the point then tap on the new location to drop the point at that location. When moving a point, there is no need to grant the change.
- To edit a line or polygon, tap a grey dot of one of the originally placed vertices, and you are provided with Move directional arrows.
- To erase a markup, tap the Remove
tool, tap a placed markup, and it’s removed.
TIP: There is no confirmation or undo option for removal. Once tapped, it’s bye-bye markup. - To remove a markup, tap Cancel
. You are prompted to confirm if you want to remove all markups.
- It is often very helpful to change the name of the current
markup session on the Job Panel by tapping the pencil
button.
- If you need to edit any attributes associated with markups
you placed, tap the right-facing arrow
to the right of a markup.
- Tap a field you want to edit. The edit behavior of each
field depends on the type of attribute you tap. Date and time fields
provide scrollable selections, whereas a text field shows a descending
character count beneath it and initiates the keyboard.
To have the current Date and Time populated, tap the Now
button.
Other available fields might initiate scrollable selections, similar to the behavior of a Date field.
TIP:-
If two or more markups overlap, and you tap on a point on the intersection of them, the item that was placed most recently is selected for editing.
-
Only one markup can be edited at a time.
-
You must finish the edit before editing a different markup.
-