Design Styles

In Designer XI, a Design Style determines the look and feel of the components in the map, including the symbols, colors, and labels. Design Styles determine the symbology for both existing components and new components that DXI you add in your design. Design Styles are the same concept as Stored Displays in the ArcFM Desktop Suite.

ArcFM Mobile supports the use of one gas and one electric .stylex Style File to display designs and operational data. Read more about using Design Styles in the DXI Using Guide.

  1. In the ArcFM Mobile app, select the desired operational map.

  2. Tap the Settings button and choose a design from the My Work tab. The selected design is then loaded in the map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?