Search for an Address

Publishes in both WPF and Xam and Android {Windows and iPad and Android}

The following steps describe how to use the Address search. You can even search for intersections, like 97th and Greene St.

  1. Xam and MAUI
    Tap the Address toggle on the Search tab. All other search options become greyed out.

  2. WPF and Xam and MAUI
    Start typing part of an address in the Search field. Suggested results start displaying underneath.
    Xam and MAUI image

  3. Xam and MAUI
    After tapping an address, a red locator is placed in the map at that address.

  4. Xam and MAUI
    Tap the at the end of the search field to clear the search results.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?