Reset Rotation

Publishes in WPF and Xam and Android

When you activate the Center on Location tool, the Reset Rotation tool is automatically activated (though it does not turn green). This tool follows as you pan and rotate, and shows you which way you’re facing relative to north. It also follows your movement when you turn the device itself in any way (or if you spin around in a chair).

The arrow always points north, and you can tap it to re-orient to north again, if needed.

This tool remains activated in offline mode, during and after an Identify, and when using the Measure tool.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?