Identify Assets at a Location

Publishes in WPF and Xam {Windows and iPad}, and profiled as such

To illustrate the way to identify an operational item, in the example below we identify a pole.

  1. Xam & MAUI- the next step goes with this one
    Tap the Identify button at the bottom right of the map, then tap on the pole in the map.
  2. Xam & MAUI
    You can optionally draw a lasso in the map. We drew a rudimentary lasso for this example.

    The list of assets within the area you draw displays under Identify, and the assets' corresponding locators appear in the map.

  3. Xam & MAUI
    Tap the right-facing arrow to view the conductor’s attributes. The conductor’s locator turns white and bounces in the map.

Publishes in Xam & MAUI
.
IMPORTANT: If your organization has configured custom tools for selected equipment, a Tasks button provides additional actions that differ based on what is configured for the identified results.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?