Diagnostics

Publishes in Xam and Android
If you ever want to make sure that a web service is accessible, or you’re wondering if a web service is why a particular package couldn’t be downloaded, this tab can help you determine a possible culprit.
  1. Tap the Settings button on the left.
  2. Tap the About tab, then tap Diagnostics.
  3. Under Test All, you can tap in the big blue circle to test all the web services that are listed on the right.

  4. After you tap Test All, the app communicates with each web service and lets you know if it could successfully reach them.

  5. You can also choose to test individual web services by tapping the play button to the left of each.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?