Send Markups

When you are finished with your markups and are ready to submit, tap the Settings button to access the My Work tab, then tap an assignment.


Depending upon how your organization has configured your tenant’s assignment types, in the right pane under Complete Job, you might see Send for Approval, as seen in the image above. Or you might see a Submit button, which sends the assignment directly back to the GIS:


The available buttons under Complete Job are entirely configurable by your administrator, so the number of available naming options is basically infinite. You might see buttons for Submit, Send for Approval, Approve/Reject, or some combination thereof.

TIP: .If your device is offline when you complete the job, the app automatically sends the markups once it detects an internet connection.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?