Measure Tool

Publishes in WPF and Xam and Android {Windows and iPad and Android} using guides

The measure tool gives you the ability to measure distances in a map in order to estimate locations in the field. The tool is located in the lower right of the app and looks like a small ruler.

Xam and Android

Xam and Android
When you tap the tool, your cursor changes in the map to a circular grey dot.

Xam and Android

Xam and Android
After you tap once in the map, two things happen:

  • The tool is activated but can be canceled.

    Xam and Android

  • A vertex is placed to start the measurement.

    Xam and Android

Both
IMPORTANT:

This tool pulls units (i.e., meters or feet) directly from the current operational map’s units. Therefore:

  • If the currently selected operational map has a coordinate system that uses the units "esriFeet," then the measurements are always in imperial measurements (feet or miles).

  • If the coordinate system uses "esriMeters" units, then the measurements are always metric (meters or kilometers).

Xam and Android
Continue tapping to place vertices.

Xam and Android

Xam and Android
As you tap, you are presented with a total distance. To start a new measurement, tap Cancel .

The tool begins to show measurements in miles or kilometers once a distance is long enough. So, if your distance is greater than 1 km, the tool starts showing you kilometers. Likewise, greater than 5,280 ft of distance provides you with measurements in miles.

Xam and Android

Xam and Android
Grab an existing vertex to move it, or tap a grey circle and move it to add a new segment.

Xam and Android

This is a very handy tool in the event that, for example, you have a fault indicator notifying you how far down a feeder that a fault has occurred.

  1. Xam and Android
    Tap to place the first vertex.

  2. Xam and Android
    Continue tapping to place vertices until you reach the desired length, then you can determine the fault location in the map.

    Xam and Android

Another handy use for this tool is when you need to find a buried switch box in a field.

  1. Xam and Android
    Tap to place the first vertex.

  2. Xam and Android
    Tap to see the sidewalk measurement.

    Xam and Android

  3. Xam and Android
    Tap again to see the total distance out in the “field.”

    Xam and Android

  4. Use both segment lengths to estimate the switch box’s location so you can access it.

TIP: While you’re using this tool, if you then select a different tool, the current measurement is cleared.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?