Tasks
Depending on the operational map you select, there are numerous possible tasks that you can perform relevant to the actions you are currently undertaking.
iPad Tasks Button
When you tap on the
Tasks button toward the bottom of the app, you may have various options
available to you, as seen in the image below. The button remains green
while activated.
Android Tasks Button
Tapping on the
Tasks button toward the bottom of the app provides various actions you
can perform, some or all of which might include those in the image
below. The button remains green while activated.
iPad Identify Tasks
When you perform an
Identify operation, after you tap the Tasks button at
the top of the Identify pane, options similar to the following might
be available to you:
To view tasks for one asset, tap the right-facing arrow to the right of the asset, then tap Tasks. You may see a menu similar to the following:
Android Identify Tasks
After performing
an Identify operation, when you tap the Tasks button at
the top of the Identify pane, you may have the following available
to you:
To view tasks for one asset, tap the right-facing arrow to the right of the asset, then tap Tasks. You may see a menu similar to the following:
iPad Trace Tasks
When you perform a
Trace, after you tap the Tasks button at the top of the Trace pane, you may
have options available to you, as seen in the following image:
Android Trace Tasks
After performing
a Trace, when you tap the Tasks button at the top of the Trace pane, the following
might be available: