Notifications

Publishes in WPF and Xam and Android {Windows and iPad and Android }

Publishes in all
Notifications provide a history of messages displayed for events, including:

  • Successful Offline Package downloads

  • Unsuccessful Offline Package downloads

  • Unsuccessful attempts to load a map

  • Removal of markup graphics from the map

Xam and Android
Tap the Notification  flag to display the Notifications pane. Individual records in the pane can be removed by tapping Dismiss next to the item. Tap Dismiss All to clear all records from the pane. To close the pane, either tap the X or the flag icon.

Xam and Android
As notifications come in, the flag appears with an exclamation by it , until you tap to dismiss them.

Publishes in all
If there are no notifications, the flag is plain grey with a green background .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?