After you have sent your current ArcFM Mobile markup session, you can view those markups and any related photos in ArcFM.

  1. In ArcFM’s Markup toolbar, click the Refresh button to view the markup you sent. Then click the Zoom to button.

  2. To view attached pictures, click the Photos button.

    You are provided with a view of all the attached photos.

  3. Click the Export button to save a zip file of all photos attached to the markup. A file browser opens, and you can name the file plus choose its save location. The photos are each named by default in the following manner: [Sequence Number] - [Job Name] - [Markup Name].
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?