Create New Program

Follow these steps to create a new program:
  1. Click the Create New Action Handler Program button.
  2. Type a name for the new program.
  3. Provide a description for the program.
  4. In the Feature Service drop-down, select which Operational Map on which you want the program to run.
  5. Click Save. The display then updates to show the new program selected in the Programs list. It also displays the Overview page and tabs for the Reconcile Events, Pre-Post Reconcile Events, and Post Events pages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.