SendEmail

An email handler allows you to set up GDBM XI to send an email when a certain event occurs. For example, it can be configured to send an email after the successful completion of a task.

Upon saving the new handler, a Properties section displays in which you can configure Recipient Email (required), Subject Text, and Email Body.

Property

Description

Recipient Email (Required)

This is the email address to which the email handler sends the automated email.

Subject Text (Optional)

This text appears in the Subject line of the email.

Email Body (Optional)

This is the text you want to include in the body of the email sent by the email handler. Tokens allow you to include specific information about the version in the body of the email. See the Tokens topic for a complete list of tokens available for use.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.