Delete Handler

If you realize you made a mistake when creating a handler, or it is no longer needed, you can easily delete it.
  1. Click on the handler in the Handlers tab list.
  2. Click the Delete button.
  3. Click Yes to confirm you want to delete the handler.

    A handler in use by a program can’t be deleted. When you try to delete a handler that’s already assigned to a program, you are notified that the handler can’t be deleted. It also indicates the programs that are currently using it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.