ExecuteGPTask

The Execute Geoprocessing Task (ExecuteGpTask) handler talks to the Geoprocessing (GP) Server that runs on the same server as the feature service where GDBM XI handles all its version management.


This is a powerful way to create a custom process (or GP Task) for feature service data triggered by GDBM activities, such as reconciling and posting versions. Examples of the custom processes are inserting rows into tables, inserting features into feature classes, modifying or deleting rows or features, and running a “version differences” process, to name a few. Almost anything that can be done to data in ArcGIS Server can be automated by a custom GP Task in a GP Server. The ExecuteGpTask handler is the go-between that allows you to program the GDBM processor to run a GP Task available on your ArcGIS Server.

As already mentioned, this handler is pretty powerful, and with great power, comes great responsibility. If you set up an ExecuteGpTask handler, you should already be familiar with authoring and publishing GP tools and have experience invoking published GP tasks through ArcGIS Server.

To set up an ExecuteGpTask handler, you start by creating a new handler as outlined in Add New Handler. After you save the new ExecuteGpTask handler, five Properties appear: GP Server Path, GP Task Name, Abort On Error, Wait for Result, and Reopen on Error. These properties need additional configuration before the handler is fully configured.

TestExecuteGpTask handler and properties

TIP: If you don’t configure properties for the ExecuteGpTask handler beyond the five initial properties, the GP Task executes with default values for any of its parameters that have been marked as required.

Property

Description

GP Server Path

The GpServerPath and GpTaskName properties are used to identify the GP Task that is invoked on the ArcGIS Server by the ExecuteGpTask handler. They help the action handler produce the correct URL for the targeted GP Task so it can invoke the GP Task via ArcGIS Server. You need to manually enter the GPServerPath and the GpTaskName into those Property fields.

Note:The GpTaskName cannot contain any spaces between the characters.

GP Task Name

Abort On Error*

The AbortOnError property is also populated with a value of true or false. It instructs the GDBM processor whether failure of the GP Task causes GDBM to stop all further processing of the current version (AbortOnError = true), or whether the processing should continue despite the failure of the ExecuteGpTask handler (AbortOnError = false).  If you do not populate the AbortOnError property, the ExecuteGpTask handler defaults to a value of false for that property.

IMPORTANT: If a value other than true or false (including an empty or misspelled value) is used for this property, the behavior of the property defaults to false.

Wait For Result

The WaitForResult property is populated with a value of true or false. This property tells the GDBM processor whether it should trigger execution of the GP Task on ArcGIS Server and return immediately (WaitForResult = false), or instead wait until the GP Task is completed (e.g., until it succeeds, fails, or times out; WaitForResult = true). If you do not populate the WaitForResult property, the ExecuteGpTask handler defaults to a value of false for that property.

Reopen On Error

The Reopen On Error property is populated with a value of true or false. If set to true, when a GP task is running on a particular version and an error occurs, the session associated with that version is reopened. That session is able to be opened again in Session Manager and participate in the next run of the GDBM processor. Within Session Manager, the session returns to the Approval assignment, and the person responsible for approving the session sees the session return in their My Work tab. Within Session History, an Audit Note says, “A conflict or error occurred during GDBM processing.” The session also appears in the Editor plugin on the Session Manager tab with a date of reopening, reason for reopening, and shows the assignment as the user who previously approved the session.

If set to false, when an error occurs on a version, the associated session is not reopened. The property is set to false by default.

The configuration of this handler is only considered when placed in a stage within the GDBM program that works on sessions/versions. If the handler is placed in the GDBM loop stage, it is ignored because the program loop works only on the default version.

IMPORTANT: By default, this property is only supported when used with the out-of-the-box Session Manager workflow. To utilize this property with custom Session Manager workflows, your custom workflow must be updated.

*The precise interpretation of AbortOnError depends upon which stage the GP action handler is in, within the GDBM Program, as outlined in the table below. The Edit Program topic contains additional information about Programs and their stages.

Stage occupied by the Action Handler in the currently running Program

Outcome when Action Handler fails and AbortOnError = true

Program Begin (both Rec & Post)

Stops the whole program. No remaining handlers in the slot fire. Program begins again next cycle, and the handlers then all get another chance.

Before Reconcile

Version is not reconciled and no remaining handlers in that slot fire for that version. Reconcile process moves on to the next version.

Before Post

Version is not posted and no remaining handlers in that slot fire for that version. Posting process moves on to the next version.

Conflict Handling

No remaining handlers in the slot fire for that version. Posting process moves on to the next version.

Error Handling (both Rec & Post)

No remaining handlers in the slot fire for that version. Posting process moves on to the next version.

After Reconcile

No remaining handlers in the slot fire for that version. Posting process moves on to the next version.

After Post

No remaining handlers in the slot fire for that version. Posting process moves on to the next version.

Program Completion

No remaining handlers in the slot fire for the program cycle that just ended.

Most GP Tasks require additional input parameters of some sort. The parameters needed to feed the GP Task everything it might need, including optional inputs, are highly variable and depend upon the design of the GP Tool that was published to ArcGIS Server to become the GP Task. At a minimum, you must add a custom property to the action handler configuration for each required parameter for the GP Task that has not been configured (when the GP Task was published) with a default value, and you must supply a value for each of those parameters in the form that the GP Task expects for them. 

You can add additional properties by clicking the Add property button next to Properties. Tokens are supported within property values if they are used in the GP Tool. See the Tokens topic for a complete list of tokens available for use.

TIP: It's helpful to be familiar with the GP Task in question via ArcGIS Server, or discussions with the original author. This can help with identifying the required and optional parameters that the GP Task may need to provide the correct names and values of the additional properties.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.