Schedules Tab

On the Schedules tab you can view scheduled entries and their details. You can also add new scheduled entries or edit existing ones.

Take it for a drive!

(That link opens/switches to the Solution Center app and accesses the Schedules tab in Geodatabase Manager XI.

Click on a day of the week to see a list of scheduled entries for that day. If you want to change the way in which these entries are displayed, refer to the Settings Tab topic for more details.

A toggle next to each scheduled entry allows you to select whether the entry runs. The Edit button allows you to make changes to the scheduled entry. The Delete button (red X) gives you the option to delete a scheduled entry from the list.

TIP: Ensure that you are certain about deleting an entry because upon deletion, the scheduled entry is immediately removed from the list without a confirmation message.

The Schedule tab also includes the Add button so you can create new scheduled entries. Refer to the Add or Edit Scheduled Entries topic for additional information about creating and editing scheduled entries.

IMPORTANT: In typically rare situations, multiple users changing the same schedule may cause issues when the system begins running scheduled events.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.