Editor Maps Tab

GDBM XI needs operational maps configured so it can connect with your data, plus run post and reconcile processes on it. The Editor Maps tab is used for configuring your operational maps. In the left pane is a list of all your previously configured operational maps.

TIP: GDBM XI and Editor XI need to share the same map service for versioning to work properly.

Take it for a drive!

(That link opens/switches to the Solution Center app and accesses the Editor Maps tab in Geodatabase Manager XI.

Follow these steps for configuration to properly work with your data:

  1. Click the Add New button to add a new operational map. This button automatically navigates you to the Operational Maps tab of the Mapping plugin to add a new operational map.
  2. Type a useful Display Name and provide the published map service URL. The URL in the image is just an example and not a working map service.


    TIP: Ensure that the URL points to a MapServer and not a FeatureServer.

  3. Use the toggles to determine which XI series applications are allowed to access the map.

  4. Under Machine-to-Machine Authentication, type the Username and Password for the ArcGIS Server/Portal for ArcGIS user credentials.

    NOTE: As a best practice, Schneider Electric recommends regularly cycling operational map machine-to-machine authentication credentials.
  5. Click Save.
  6. Click the back arrow at the top left of the Solution Center window to return to the Editor Maps tab.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.