GDBM XI Licenses

Geodatabase Manager (GDBM) XI works in parallel with your organization’s overall licensing terms. Some GDBM activities use a license seat when running, such as scheduled entries. This means the number of activities you can run simultaneously is dependent on the number of seats your organization owns. For example, if you have Electric GDBM processing scheduled for 5 p.m. - 9 p.m., and Gas GDBM processing scheduled from 9 p.m. -1 a.m., without overlap, you need only one license of GDBM. If you schedule both to run from 5 p.m. - 9 p.m., then you need two licenses.

IMPORTANT: Licenses are managed at the tenant level. If you have multiple tenants, each tenant requires a GDBM license.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.