DeleteVersionAfterPost

This handler deletes the version being processed, and it times out after two minutes by default. You can customize the Times Out After setting to a time that best suits your needs.

Property

Description

Delete Session Associated With Deleted Version

When set to true, this also deletes the associated session. False is the default.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.