Prerequisites for GDBM

Geodatabase Manager (GDBM) XI is a plugin for Solution Center. Given that its purpose is to automate tasks for maintaining a continuously up-to-date Utility Network (UN), GDBM integrates with other XI series apps, rather than operating as a stand-alone app.

The following are required before the implementation process can begin:

  • It is assumed that you have completed an Online Service Agreement and requested a tenant. Please contact your Account Manager for more information. For more information, read the Security Considerations and Request a Tenant topics.

  • Ensure that the necessary applications are at a supported version and license level. For the most up-to-date information about supported versions and licenses, visit the GDBM XI Supported Versions article on myArcFM.

  • Review the ArcFM Solution XI Series Named User Functionality Matrix. This information is useful later as you configure tenant authentication. For more information, read the Configure Tenant Authentication topic.

  • Review the ArcFM UN Configuration Guide. To ensure a smooth implementation of GDBM, your UN data model should adhere as closely as possible to this configuration.

  • Feeder Services consumes GDBM action handlers as a part of its Geodatabase Region Resource (GRR) creation/update scheduling procedure. Refer to the GDBM XI Licenses topic for information about GDBM licensing.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.