Tokens

The following table describes the tokens available for use in GDBM XI:

Token

Description

{Action}

The GDBM slot name (i.e., Before Post, After Reconcile) in which the handler has been applied in a program.

{ErrorDetail}

Details of any errors that might occur at any point in the session’s lifecycle.

{FeatureService}

URL to the feature service the program is configured with.

{SessionApprover}

Name of the user who can approve/reject a session.

{SessionCreatedDate}

Date the session was initiated.

{SessionDescription}

Descriptive information about the session that the SessionApprover needs to know.

{SessionName}

A recognizable name for the current session.

{SessionOwner}

Name of the user who initiated the session.

{SessionPostedDate}

Date that the session moved from the posting queue to being posted.

{SessionPostQueuedDate}

Date that the session was sent to the queue for posting.

{Tenant}

The Tenant name running GDBM XI.

{Version}

Name of the version being processed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.