Delete Program

Follow these steps to delete a program:
  1. Select the program you want to delete in the Programs tab list.
  2. On the Overview page, click the Delete button in the bottom left of the page.
  3. Click Yes to confirm you want to delete the program.

    Programs can be deleted from GDBM XI if they have already been used in a scheduled entry. When you try to delete a program that’s already scheduled to run on a specific date, you are notified with a message stating the program can’t be deleted, and the day and time at which it is scheduled to run is provided.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.