Appendix 1: Sepam current input connection diagrams
Phase current input connection schemes
The current input connection of the existing Sepam protection relay could be done according to one of the following diagrams
|
Variant 1: phase current measurements by 3 x 1 A or 5 A CTs (standard connection) |
|||||||
|
Description Connection of 3 x 1 A or 5 A sensors to the CCA630 or CCA634 connector. The measurement of the 3 phase currents allows the calculation of residual current. Parameters
|
|||||||
|
Variant 2: phase current measurement by 2 x 1 A or 5 A CTs |
|||||||
|
Description Connection of 2 x 1 A or 5 A sensors to the CCA630 or CCA634 connector. The measurement of phase currents 1 and 3 is sufficient to help ensure all the phase current based protection functions. The phase current I2 is only assessed for metering functions, assuming that I0 = 0. This arrangement does not allow the calculation of residual current. Parameters
|
|||||||
|
Variant 3: phase current measurement by 3 LPCT type sensors |
|||||||
|
Description Connection of 3 Low Power Current Transducer (LPCT) type sensors to the CCA670 connector. The connection of only one or two LPCT sensors is not allowed and causes Sepam to go into fail-safe position. The measurement of the 3 phase currents allows the calculation of residual current. Parameters
|
|||||||
Residual current input connection schemes
The residual current input connection of the existing Sepam protection relay could be done on connector B (CCA 630/CCA634/CCA670) and connector A according to one of the following diagrams:
|
Variant 1: residual current calculation by sum of 3 phase currents |
||||||||||
|
Description Residual current is calculated by the vector sum of the 3 phase currents I1, I2 and I3, measured by 3 x 1 A or 5 A CTs or by 3 LPCT type sensors. See current input connection diagrams. Parameters
|
||||||||||
|
Variant 2: residual current measurement by CSH120 or CSH200 core balance CT (standard connection) |
||||||||||
|
Description Arrangement recommended for the protection of isolated or compensated neutral systems, in which very low fault currents need to be detected. Parameters
|
||||||||||
|
Variant 3: residual current measurement by 1 A or 5 A CTs and CCA634 |
||||||||||
|
Description Residual current measurement by 1 A or 5 A CTs.
Parameters
|
||||||||||
|
Variant 4: residual current measurement by 1 A or 5 A CTs and CSH30 interposing ring CT |
||||||||||
|
Description The CSH30 interposing ring CT is used to connect 1 A or 5 A CTs to Sepam to measure residual current:
Parameters
|
||||||||||
|
Variant 5: residual current measurement by core balance CT with ratio of 1/n (n between 50 and 1500) |
||||||||||
|
Description The ACE990 is used as an interface between an MV core balance CT with a ratio of 1/n (50 < n < 1500) and the Sepam residual current input. This arrangement allows the continued use of existing core balance CTs on the installation. Parameters
|
||||||||||