JYT8754702–01

Material Not Included in the Kit

Comb-busbar

The comb-busbar can be used to optimize the installation, for example by creating rapidly a common point for digital inputs.

To facilitate wiring the terminals X3, X4, X5 of PowerLogic P3 protection relay, the user can order the following comb-busbar 50-piece or 100-piece packs.

Commercial reference

Description

Quantity/pack

Illustration

REL51054

2-pin comb-busbar

100 pieces

REL51055

3-pin comb-busbar

100 pieces

REL51056

4-pin comb-busbar

50 pieces

REL51057

5-pin comb-busbar

50 pieces

REL51058

6-pin comb-busbar

50 pieces

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?