JYT8754702–01

Materials and Information Prerequisite

Questionnaire

A questionnaire is to be generated by the EcoFit Conversion Tool, a software that comes with the EcoFit offer for converting Sepam settings into new setting files usable on the EcoFit protection relay.

This questionnaire collects the technical information from the existing application and can help the installer to get familiar with the existing installation environment and thus minimize the down time caused by the replacement.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?