JYT8754702–01

Rear Panel Mask

The rear panel mask is to be pasted on the rear panel of the PowerLogic P3 protection relay. It is intended for marking out the used terminals of the Sepam protection relay on the PowerLogic P3 protection relay and thus mimicking the original application scenario.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?