JYT8754702–01

Front Panel Description

The PowerLogic P3 protection relay provided with the installation kit is PowerLogic P3U30 model.

  1. LCD

  2. Navigation push-buttons

  3. Object control buttons

  4. LED indicators

  5. Local port

  6. Function push-buttons and LEDs showing their status

  7. INFO push-button

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?