JYT8754702–01

Wire Stickers

The wire stickers are printed with the terminal numbers of both the Sepam protection relay and the PowerLogic P3 protection relay.

They are intended for labelling the wires disconnected from the Sepam protection relay and are to be re-connected to the PowerLogic P3 protection relay.

By checking the wire sticker, the installer quickly singles out the PowerLogic P3 terminal to which the wire needs to be connected.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?