JYT8754702–01

Labelling the Wires

To help re-connect the PowerLogic P3 protection relay quickly and correctly, wire stickers are designed and provided in the installation package.

To label the wires on the Sepam protection relay, proceed as follows:

  1. Prepare a wiring diagram of the Sepam protection relay.
  2. WARNING
    hazard of incorrect wiring
    • To ensure the correct wiring of the PowerLogic P3 protection relay based on the original wiring scheme, pick up the wire sticker with the correct Sepam terminal number. Otherwise, when wiring the PowerLogic P3 later, the wire will be connected to the wrong PowerLogic P3 terminal.
    • Pay attention to the common connections.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  3. Select a connection and mark it out on the wiring diagram.
  4. Single out the corresponding wire on the Sepam according to the terminal number on the wiring diagram.
  5. Press the wire sticker on the wire end as shown in the following figure.
  6. Repeat the above steps to label the other wires.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?