JYT8754702–01

Removing the Communication Interface

The Sepam protection relay uses a communication interface to connect to the network. The interface can be located in the LV compartment or equipment rack. The PowerLogic P3, on the other hand, can be directly connected to the network using a communication cable.
NOTE: Different type of interface can be used for the Sepam protection relay. The following removal process uses one of the interfaces as an example.
  1. Locate the communication interface used for the Sepam protection relay in the LV compartment or equipment rack.
  2. Disconnect the cable (1) and wires (2) from the interface, and using a screwdriver disconnect the earthing wire (3).
  3. Place the disconnected cable and wires temporarily in the de-energized LV compartment or equipment rack.
  4. Disengage and remove the communication interface from the DIN rail.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?