JYT8754702–01

Introduction to the PowerLogic P3 Protection Relay Assembly

The assembly of the PowerLogic P3 protection relay on the equipment is performed in two main steps:

  1. Mounting the PowerLogic P3 protection relay in its case.

  2. Assembling the PowerLogic P3 protection relay case on the equipment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?