JYT8754702–01

Mounting Case

The mounting case is used as an adapter case for installing the PowerLogic P3 protection relay at the existing Sepam installation location.

Due to different mounting dimensions, the PowerLogic P3 protection relay cannot be directly installed at this location without this mounting case.

  1. Box

  2. Frame

  3. Side covers

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?