JYT8754702–01

Rear Terminal Designation

PowerLogic P3U30 Rear Panel – 3CT 1Io or 3CT CSH / 4VT RS485

PowerLogic P3U30 Rear Panel – 3CT 1Io or 3CT CSH / 4VT 2 RJ45

PowerLogic P3U30 Rear Panel – 3LPCT CSH / 4LPVT RS485

PowerLogic P3U30 Rear Panel – 3LPCT CSH / 4LPVT 2 RJ45

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?