Appendix 2: Sepam voltage input connection diagrams
Sepam series 20
The phase and residual voltage transformer secondary circuits are connected to the connector B (CCT640) on Sepam series 20 protection relays according to one of the following connection diagrams.
|
Variant 1: measurement of 3 phase-to-neutral voltages (standard connection) |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 2: measurement of 3 phase-to-neutral voltages and residual voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 3: measurement of 2 phase-to-phase voltages |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 4: measurement of 1 phase-to-phase voltage and residual voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 5: measurement of 1 phase-to-phase voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
Sepam series 40
The phase and residual voltage transformer secondary circuits are connected directly to the connector E (CCA626/CCA627) on Sepam series 40 protection relay according to one of the following connection schemes.
|
Variant 1: measurement of 3 phase-to-neutral voltages (standard connection) |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 2: measurement of 2 phase-to-phase voltages and residual voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 3: measurement of 2 phase-to-phase voltages |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 4: measurement of 1 phase-to-phase voltage and residual voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||
|
Variant 5: measurement of 1 phase-to-phase voltage |
|||||||||||||
|
Parameters
Functions available
|
|||||||||||||