JYT8754702–01

Required Tools

The following tools are needed for the replacement operations:

  • Screwdriver with torque indication, equipped with the following screw tips:

    • 6.5 mm (1/4 in) flat blade tip, or PZ2 tip

    • 2.5 mm (3/32 in) flat blade tip

  • Spanner with torque indication, equipped with M4 socket tip

  • Voltage detector

  • Multimeter

  • Wire cutting and stripping pliers

  • Crimping pliers

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?