Applications
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not use a G0110 residual current sensor with the EcoFit
PowerLogic P3 solution.
Failure to follow these instructions will result in death or serious injury.
|
The table below lists the applications of the EcoFit solution, to replace Sepam series 20 or 40 protection relays by PowerLogic™ P3 protection relays.
|
Sepam 20 |
PowerLogic P3U30 |
|---|---|
|
S20 /S23 / S24 |
P3U30 |
|
T20 / T23 / T24 |
P3U30 |
|
M20 |
P3U30 |
|
B21 / B22 |
P3U30 |
|
Sepam 40 |
PowerLogic P3U30 |
|---|---|
|
S40 / S41 / S42 / S43 / S44 |
P3U30 |
|
S50 / S51 / S52 / S53 / S54 |
P3U30 |
|
M40 / M41 |
P3U30 |
|
G40 |
P3U30 |
DANGER