JYT8754702–01

Finalize the Installation

The following operations are needed to properly finalize the installation:

  • Check that all the cables and wires are correctly connected to the PowerLogic P3 protection relay according to the wiring labels and diagrams. Refer to the wiring diagram provided by the customer, or the wiring diagrams appended at the end of this guide

  • Check that all the connections are tightened with the specified torque.

  • Check that no parts or accessories, tools, or other foreign materials have been left in the LV compartment or equipment rack.

  • Close the LV compartment door or any covers of the equipment rack.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?