DOCA0178EN-22

Major Fixes for Firmware Version 002.006.000

  • The password reset issue that occurred in rare cases in firmware version 002.005.000 has been fixed.

  • The issue reported for Panel Server with firmware version 002.005.000, related to the Settings webpage for the PowerTag Control IO device (A9XMC1D3) that may be inaccessible on Panel Server webpages after a restore operation on Panel Server, has been fixed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.