DOCA0178EN-22

Limitations for Firmware Version 002.006.000

Limitations on Wi-Fi Communication

  • The limitation described in the following table applies to all Panel Server models with firmware version 002.006.000, except Wired by Design models (PAS600LWD, PAS600PWD), when:

    • the Wi-Fi infrastructure is configured on the Panel Server webpages, and

    • Panel Server is connected to a Wi-Fi access point.

If... Then... Action
  1. the user disables the Wi-Fi infrastructure from the Panel Server webpages (Infrastructure activation and Wi-Fi activation disabled), and

  2. the user applies the changes by clicking the Save & apply configuration button

Panel Server cannot reconnect through the Ethernet interface by default, hence:

  • the user can no longer connect to the webpages,

  • Panel Server cannot publish data to the Schneider Electric cloud or an SFTP or HTTPS server by using the Ethernet interface (in either configured Ethernet mode, Separated or Switched).

  • Power off then power on the Panel Server by using the multifunction button on the Panel Server front face. For more information about Multifunction Button, refer to DOCA0172•• EcoStruxure Panel Server - User Guide, or

  • Unplug then plug again the power wire from the Panel Server power supply terminal block.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.