Architecture Examples
FDM128 Display Connected to an IFE Server
The following diagram is an example of an IFE- based network architecture:
|
A |
FDM128 Ethernet display for eight devices |
H |
EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker |
|
B |
IFE Ethernet switchboard server |
I |
ULP line termination |
|
C |
IFM Modbus-SL interface for one circuit breaker |
J |
ULP cord |
|
D |
FDM121 ULP display for one circuit breaker |
K |
NSX cord |
|
E |
I/O input/output application module for one circuit breaker |
L |
Smartlink Modbus gateway |
|
F |
MasterPacT MTZ drawout circuit breaker |
Ethernet |
|
|
G |
Modbus-SL |
||
|
24 Vdc |
FDM128 Display Connected to an Smartlink SI B Gateway
The following diagram is an example of an Smartlink SI B network architecture, in a floor switchboard application:
FDM128 Display Connected to an Smartlink SI D Gateway
The following diagram is an example of an Smartlink SI D wireless network architecture, in a floor switchboard application:
FDM128 Display Connected to an EcoStruxure Panel Server
The following diagram is an example of an EcoStruxure Panel Server wireless network architecture, in a floor switchboard application:
FDM128 Display Connected to a PowerLogic EGX300 or EGX100 Ethernet Gateway
The following diagram is an example of a network architecture with a PowerLogic EGX300 Ethernet gateway:
|
A |
FDM128 Ethernet display for eight devices |
I |
ULP line termination |
|
B |
ConneXium switch |
J |
ULP cord |
|
C |
EGX300 Ethernet gateway |
K |
BCM ULP |
|
D |
IFM Modbus-SL interface for one circuit breaker |
L |
NSX cord |
|
E |
FDM121 ULP display for one circuit breaker |
M |
Smartlink Modbus gateway |
|
F |
CCM Modbus cradle communication module |
Ethernet |
|
|
G |
MasterPacT NT/NW circuit breaker |
Modbus-SL |
|
|
H |
24 Vdc |
FDM128 Display Connected to Several IFE, Smartlink SI B , Smartlink SI D , or EcoStruxure Panel Server Gateways
The following diagram is an example of an IFE- and Smartlink SI B , Smartlink SI D , EcoStruxure Panel Server-based network architecture:
|
A |
FDM128 Ethernet display for eight devices |
J |
NSX cord |
|
B |
ConneXium switch |
K |
PowerTag energy sensor |
|
C |
IFE Ethernet interface for one circuit breaker |
L |
PowerTag Link |
|
D |
I/O input/output application module for one circuit breaker |
M |
EcoStruxure Panel Server |
|
E |
MasterPacT MTZ fixed circuit breaker |
Ethernet |
|
|
F |
24 Vdc |
||
|
G |
Smartlink SI B gateway |
TI24 cord |
|
|
H |
ULP cord |
110/230 Vac |
|
|
I |
ULP line termination |
FDM128 Display Connected to Several Gateways
The following diagram is an example of architecture where the FDM128 display is connected to several gateways:
|
A |
FDM128 Ethernet display for eight devices |
J |
Smartlink Modbus gateway |
|
B |
IFE Ethernet switchboard server |
K |
EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker |
|
C |
IFM Modbus-SL interface for one circuit breaker |
L |
ULP cord |
|
D |
I/O input/output application module for one circuit breaker |
M |
NSX cord |
|
E |
MasterPacT MTZ drawout circuit breaker |
N |
PowerTag energy sensor |
|
F |
Ethernet |
||
|
G |
ConneXium switch |
Modbus-SL |
|
|
H |
ULP line termination |
24 Vdc |
|
|
I |
Smartlink SI B gateway |
TI24 cord |
Component Part Numbers
The following table lists the part numbers for the components in the architecture diagrams:
|
Component |
Description |
Part Number |
|---|---|---|
|
FDM128 Ethernet display for eight devices |
– |
LV434128 |
|
STU 5in7 front module spare part |
– |
HMIS85 |
|
IFE Ethernet interface for one circuit breaker |
– |
LV434001 |
|
IFE Ethernet switchboard server |
– |
LV434002 |
|
EIFE embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker |
EIFE embedded Ethernet interface |
LV851001 |
|
Spare part kit EIFE for one MasterPacT MTZ1 drawout circuit breaker |
LV851100SP |
|
|
Spare part kit EIFE for one MasterPacT MTZ2/MTZ3 drawout circuit breaker |
LV851200SP |
|
|
IFM Modbus-SL interface for one circuit breaker |
– |
LV434000 |
|
FDM121 ULP display for one circuit breaker |
– |
|
|
I/O input/output application module for one circuit breaker |
– |
LV434063 |
|
ULP line termination |
10 ULP line terminations |
TRV00880 |
|
ULP cord |
L = 0.3 m (0.98 ft) |
TRV00803 |
|
L = 0.6 m (1.97 ft) |
TRV00806 |
|
|
L = 1 m (3.28 ft) |
TRV00810 |
|
|
L = 2 m (6.56 ft) |
TRV00820 |
|
|
L = 3 m (9.84 ft) |
TRV00830 |
|
|
L = 5 m (16.40 ft) |
TRV00850 |
|
|
BCM ULP cord |
L = 0.35 m (1.15 ft) |
LV434195 |
|
L = 1.3 m (4.26 ft) |
LV434196 |
|
|
L = 3 m (9.84 ft) |
LV434197 |
|
|
TI24 cord |
- |
A9XCAS06 |
|
NSX cord |
L = 0.35 m (1.15 ft) |
LV434200 |
|
L = 1.3 m (4.27 ft) |
LV434201 |
|
|
L = 3 m (9.84 ft) |
LV434202 |
|
|
PowerTag Link – Wireless to Modbus TCP/IP Concentrator |
A9XMWD20 |
|
|
PowerTag Link HD – Wireless to Modbus TCP/IP Concentrator |
A9XMWD100 |
|
|
PowerTag Link B gateway |
– |
A9XMZC20 |
|
Smartlink Modbus gateway |
Smartlink – Modbus RS485 slave – Smart Communication I/O Module |
A9XMSB11 |
|
Smartlink SI B gateway |
Smartlink SI B – Modbus TCP/IP and Wireless Communication Module |
A9XMZA08 |
|
Smartlink SI D gateway |
Smartlink SI D – Wireless to Modbus TCP/IP Concentrator |
A9XMWA20 |
|
EcoStruxure Panel Server Universal |
Wireless Concentrator and Modbus Gateway, Datalogger and Energy Server |
– |
|
24 Vdc |
PAS600L |
|
|
110–240 Vac/Vdc |
PAS600T |
|
|
110–277 Vac/Vdc |
PAS600 |
|
|
PoE (Power over Ethernet) |
PAS600P |
|
|
EcoStruxure Panel Server Advanced |
Wireless Concentrator and Modbus Gateway, Datalogger and Energy Server |
– |
|
24 Vdc |
PAS800L |
|
|
110–277 Vac/Vdc |
PAS800 |
|
|
PoE (Power over Ethernet) |
PAS800P |
|
|
EcoStruxure Panel Server Entry |
Wireless Concentrator Gateway |
– |
|
110–277 Vac/Vdc |
PAS400 |
|
|
PowerLogic EGX300 Ethernet gateway |
– |
|
|
iEM2000T energy meter |
Single-phase energy meter without display |
A9MEM2000T |
|
iEM3110 energy meter |
Three-phase energy meter with display |
A9MEM3110 |
|
iEM3155 energy meter |
Three-phase energy meter with display |
A9MEM3155 |
|
iEM3210 energy meter |
Three-phase energy meter with display |
A9MEM3210 |
|
iEM3255 energy meter |
Three-phase energy meter with display |
A9MEM3255 |
|
PowerTag energy Monoconnect 63 A |
PowerTag energy M63 1P+wire |
A9MEM1520 |
|
PowerTag energy M63 1P+N Top |
A9MEM1521 |
|
|
PowerTag energy M63 1P+N Bottom |
A9MEM1522 |
|
|
PowerTag energy M63 3P |
A9MEM1540 |
|
|
PowerTag energy M63 3P+N Top |
A9MEM1541 |
|
|
PowerTag energy M63 3P+N Bottom |
A9MEM1542 |
|
|
PowerTag energy M63 3P 230 V LL |
A9MEM1543 |
|
|
PowerTag energy Flex 63 A |
PowerTag energy F63 1P+N |
A9MEM1560 |
|
PowerTag energy F63 1P+N 110 V |
A9MEM1564 |
|
|
PowerTag energy F63 3P+N |
A9MEM1570 |
|
|
PowerTag energy F63 3P |
A9MEM1573 |
|
|
PowerTag energy PhaseNeutral 63 A |
PowerTag energy P63 1P+N Top |
A9MEM1561 |
|
PowerTag energy P63 1P+N Bottom |
A9MEM1562 |
|
|
PowerTag energy P63 1P+N Bottom for RCBO 18 mm |
A9MEM1563 |
|
|
PowerTag energy P63 3P+N Top |
A9MEM1571 |
|
|
PowerTag energy P63 3P+N Bottom |
A9MEM1572 |
|
|
PowerTag energy F63 3P+N 127/220 V |
A9MEM1574 |
|
|
PowerTag energy Flex 160 A |
PowerTag energy F160 3P/3P+N |
A9MEM1580 |
|
PowerTag energy Rope 200 A |
PowerTag energy R200 3P/3P+N |
A9MEM1590 |
|
PowerTag energy Rope 600 A |
PowerTag energy R600 3P/3P+N |
A9MEM1591 |
|
PowerTag energy Rope 1000 A |
PowerTag energy R1000 3P/3P+N |
A9MEM1592 |
|
PowerTag energy Rope 2000 A |
PowerTag energy R2000 3P/3P+N |
A9MEM1593 |
|
PowerTag energy Monoconnect 250 A |
PowerTag energy M250 3P |
LV434020 |
|
PowerTag energy M250 4P |
LV434021 |
|
|
PowerTag energy Monoconnect 630 A |
PowerTag energy M630 3P |
LV434022 |
|
PowerTag energy M630 4P |
LV434023 |
|
|
PowerTag NSX energy sensor 250 A (China market only) |
PowerTag NSX 250 3P |
LVSMC13 |
|
PowerTag NSX energy sensor 630 A (China market only) |
PowerTag NSX 630 3P |
LVSMC23 |





Note for TechPub writer: part of information in this block is common with D-SE-0039082.1.13 (FDM121 guide).