Prerequisites
Ethernet Network
The Ethernet connections of the IP devices in the Ethernet network must be correctly installed and configured.
The Ethernet network may include the following IP devices:
-
EGX300 or EGX100 gateways
-
Link150 gateways
-
IFE or EIFE interfaces
-
IFE server
-
Smartlink Ethernet devices
-
Smartlink SI B gateway
-
Smartlink SI D gateway
-
PowerTag Link gateway
-
PowerTag Link B gateway
- PowerTag Link HD gateway
-
Third-party gateways
-
EcoStruxure Panel Server Universal
-
EcoStruxure Panel Server Advanced
-
EcoStruxure Panel Server Entry
For further information, refer to the corresponding user guides provided in the section Related Documents.
Modbus Serial Line Network
The devices in the Modbus serial line network must be correctly installed and configured with the following Modbus parameters:
|
Parameter |
Value |
|---|---|
|
Modbus address (slaves only) |
The Modbus address of each monitored device must be unique. The range of Modbus addresses is [1-247]. |
|
Physical interface |
RS-485 2-wire |
|
Transmission mode |
RTU (Automatic) |
|
Communication speed |
The communication speed must be the same for all devices. |
|
Parity |
The parity must be the same for all devices. |
|
Response time-out |
1 second |
To check the Modbus parameters of each monitored device, refer to the section Related Documents:
-
The BCM ULP Circuit Breaker Communication Module Installation Manual
-
The IFM Modbus-SL Interface for One Breaker - Instruction Sheet
-
The Smartlink Modbus Communication System User Manual
Architecture Network Limitation
The limitations of the architecture network are as follows:
-
Modbus serial line time out in the IFE device should be 1 s.
-
To avoid communication error or not to overload the network, a maximum of two FDM128 displays must be connected to the same IFE device. The FDM128 displays can scan data of the same circuit breaker.