Firmware Update
Firmware Update Policy
The primary reason for updating the firmware of a FDM128 display is to obtain the latest FDM128 features. If the latest FDM128 features are not required, it is not mandatory to update the firmware of FDM128 display.
If you notice a bug on the FDM128 display, refer to FDM128 firmware release note to check if the bug is corrected in a later version of the firmware. Update the firmware of the FDM128 display to benefit from the correction. If there is no bug fix available, call the Customer Care Centre.
Prerequisites
To update the FDM128 firmware, use a USB memory key.
This USB memory key must be:
-
Formatted in FAT32 system format
-
Empty
DANGER |
|---|
|
RISK OF ELECTROCUTION, ELECTRIC ARC, OR BURNS
Failure to follow these instructions will result in death or serious injury.
|
Downloading the Latest Firmware Version
Perform the below steps to download the latest firmware version:
|
Step |
Action |
|---|---|
|
1 |
Go to the Schneider Electric home page www.se.com. |
|
2 |
In the box, type the reference of the
FDM128 display
(
|
|
3 |
If you entered the reference, go to the search results. If you entered the name of the product offer, go to the search results. Click the link of the FDM128 display product. |
|
4 |
Click , then go to section. The list of available firmware for the FDM128 display is displayed. |
|
5 |
Click the link of the FDM128 firmware version you want to download. Save the .zip file on your computer. |
Updating the Firmware
WARNING |
|---|
|
LOSS OF DATA
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
After downloading the firmware, update the FDM128 display as follows:
DANGER
WARNING