Setting Wizard
Wizard Presentation
A setting wizard is automatically launched at first power-on to help you set up the FDM128 display .
The setting wizard guides you through three main configuration parts:
-
FDM128 display general settings
-
Communication settings depending on the network architecture
-
Editing device function
Each configuration part is described further in this section.
It is recommended that you update the communication settings each time you modify the communication network.
General Settings
The following table describes the sequence of steps presented by the setting wizard to configure the FDM128 general settings:
|
Step |
Screen |
Action |
|---|---|---|
|
1 |
Welcome |
Touch the screen to start the wizard. |
|
2 |
|
Select a language. |
|
3 |
|
Press one of the two possible ways to set manually the real-time sample rate in the :
Example:
|
|
4 |
|
Press one of the two possible ways to represent the phases 1,2,3,N (default setting), or A,B,C,N. |
|
5 |
|
Select the units of measurement for the analog input of the I/O modules:
|
|
6 |
|
Press the -/+ icons to adjust the brightness level of the display. In the footer, press Finish. The setting wizard displays the screen to allow you to set up the FDM128 communication. Follow the communication settings procedure that corresponds to your network architecture. |
Communication Settings for a Single Gateway-Based Architecture
This procedure is applicable when:
-
The FDM128 display is connected to an IFE interface or an EIFE interface
-
The FDM128 display is connected to an Smartlink SI B or Smartlink SI D gateway
-
The FDM128 display is connected to an EcoStruxure Panel Server
-
The FDM128 display is connected to an EGX gateway
The FDM128 setting wizard guides you through the following steps:
|
Step |
Action |
|---|---|
|
1 |
Configure the FDM128 display within the network. Set the following parameters:
|
|
2 |
Press to indicate that the FDM128 display is connected to a gateway. |
|
3 |
Set the IP address of the gateway. |
|
4 |
Enter between 1–247. |
|
5 |
Press to launch the device discovery sequence. For more information, refer Device Discovery. Up to 16 devices are displayed. |
|
6 |
Select up to eight devices among the devices displayed. |
|
7 |
If you select less than eight devices among the devices displayed, you are prompted for an additional gateway. Press . |
|
8 |
If needed, you can configure manually extra IFE, EIFE, Smartlink SI B , or Smartlink SI D devices. |
|
9 |
Press . The FDM128 display can now monitor the list of selected devices. The setting wizard displays the screen to allow you to edit the label and name of the devices. |
in step 8 in the table above, for DTP team, on SPANISH language: if the sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
Communication Settings for Several Gateway-Based Architectures
This procedure is applicable when the FDM128 display is connected to several gateways.
The FDM128 setting wizard guides you through the following steps:
|
Step |
Action |
|---|---|
|
1 |
Configure the FDM128 display within the network. Set the following parameters:
|
|
2 |
Press to indicate that the FDM128 display is connected to a gateway. |
|
3 |
Set the IP address of the gateway. |
|
4 |
Enter between 1–247. |
|
5 |
Press to launch the device discovery sequence Device Discovery. Up to 16 devices are displayed. |
|
6 |
Select up to eight devices among the devices displayed. |
|
7 |
If you select less than eight devices among the devices displayed, you are prompted for an additional gateway. If you have another gateway to configure, press and go back to step 3. |
|
8 |
When you have configured all gateways, press . You can now manually configure extra IFE, EIFE, Smartlink SI B , or Smartlink SI D devices. |
|
9 |
Press . The FDM128 display can now monitor the list of selected devices. The setting wizard displays the screen to allow you to edit the label and name of the devices. |
In step 8 in the table above, for DTP team, on SPANISH language: if the sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
Communication Settings for Several IFE, EIFE, Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server Architecture
The procedure is applicable when the FDM128 display is connected to several IFE, EIFE , Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server devices.
The FDM128 setting wizard guides you through the following steps:
|
Step |
Action |
|---|---|
|
1 |
Configure the FDM128 display within the network. Set the following parameters:
|
|
2 |
Press to indicate that there is no gateway. |
|
3 |
Configure manually up to eight IFE, EIFE, Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server devices. |
|
4 |
Press . The FDM128 display can now monitor the list of selected devices. The setting wizard displays the screen to allow you to edit the label and name of the devices. |
In step 4 in the table above, for DTP team, on SPANISH language: if the sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
Device Discovery
The device discovery feature enables detection of devices in a given Modbus range (1–247).
The device discovery sequence detects up to 16 devices on the network as per the given Modbus range. These devices are displayed sorted in ascending order of Modbus address, with the Modbus address indicated in the first column.
The device discovery sequence time varies depending on the Modbus range selected.
Among the detected devices, you can select a maximum of eight devices.
for DTP team, on SPANISH language: if following sentence starts with "unidad de visualizacion....", set a capital 'U' so that it reads "Unidad de visualizacion"
The FDM128 display guides you through the following device discovery procedure:
|
Step |
Action |
|---|---|
|
1 |
The device discovery sequence is started during the communication settings procedure. A progress bar is displayed during the device discovery sequence. NOTE: During the device discovery, if you want to stop the discovery
sequence, press . It will take you back to the page.
|
|
2 |
In the list of the discovered devices, select the check box for each device you want to include. Devices previously selected in a device discovery loop are displayed in gray. |
|
3 |
Press . The screen appears. |
Manual Configuration of IFE, EIFE, Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server Gateways
You configure devices manually either after a device discovery sequence, or if you do not have a IFE, EIFE, Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server gateway.
To configure devices manually during the device settings sequence, proceed as follows:
|
Step |
Action |
|---|---|
|
1 |
|
|
2 |
For each selected device, set its IP address. |
|
3 |
Press to launch the device discovery sequence. Device Discovery page is displayed with the list of available gateways. NOTE: A maximum of 8 devices can be discovered.
|
|
4 |
Select up to eight devices among the devices displayed. |
|
5 |
If you select less than eight devices among the devices displayed, you are prompted for an additional gateway. Press . |
|
6 |
If needed, you can configure manually extra IFE, EIFE, Smartlink SI B , Smartlink SI D , PowerTag Link, or EcoStruxure Panel Server devices. |
|
7 |
Press . The FDM128 display can now monitor the list of selected devices. The setting wizard displays the screen to allow you to edit the label and name of the devices. |
Power Loss
In case of power loss, the FDM128 display retains the settings.


@Tech Pub writer/translator: the screen names in the table below are all in the file Vijeo-DesignerLanguages.xlsx (HMI terms for FDM128, translated) except "Welcome". The terms in the XSLX file are preceeded by "Settings / <num>." where <num> is a number different for each.