DOCA0037EN-13

Regular Cleaning

Cleaning the Display

NOTICE
EQUIPMENT DAMAGE
  • Power off the FDM128 display before cleaning it.
  • Do not use hard or sharp objects to operate the touch panel since it can damage the panel surface.
  • Do not use paint thinner, organic solvents, or a strong acid compound to clean the FDM128 display .
Failure to follow these instructions can result in equipment damage.

When the surface or the frame of the display gets dirty, soak a soft cloth in water with a neutral detergent, wring the cloth tightly, and wipe the display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?