Real-Time Alarms
Overview
Alarms are displayed differently according to their priority level.
Alarms for Circuit Breakers
The circuit breaker predefined alarms are displayed on the FDM128 display as follows:
|
Alarm Priority |
Description |
|---|---|
|
Trip |
When a trip occurs, the FDM128 screen shows a pop-up window. The following window represents an example of a trip on circuit breaker CB01. You must close this window before returning to the . This alarm also appears as a red icon on the screen and on the title bar of the screen. |
|
High |
The device icon turns red to indicate a high-priority alarm Icon Mode. This alarm also appears as a red icon on the title bar of the screen. |
|
Medium |
When a medium-priority alarm occurs, an orange icon appears on the screens and on the title bar of the screens. |
|
Low |
Low-priority alarms are only registered in the alarm history and viewable in the submenu. |
Alarms for Circuit Breakers Connected to Smartlink SI B Device
Alarms are raised depending on the type of circuit breaker:
-
Acti9 circuit breakers: when an alarm occurs, the FDM128 screen shows a pop-up window. You must close this window before returning to the . This alarm also appears as a red icon on the screen and in the corresponding Smartlink SI B and Smartlink Modbus ().
-
Other circuit breakers: an alarm appears as a red icon on the screen and in the corresponding ().
An example of this type of circuit breaker is item C in the architecture diagram showing the FDM128 display connected to an Smartlink SI B .
General View Grid Screen Icons
|
Icon Color |
Description |
|---|---|
|
Red |
There is an active alarm with a high severity or the circuit breaker has tripped. |
|
Partial orange (current value and ID are displayed) |
A medium severity alarm is active. |
|
Full orange (only ID is displayed) |
FDM128 display has lost the communication with the circuit breaker. Check the cable connection or check if the Modbus serial line time out is set to 1 s. |
|
Full orange (ID and disconnected symbols are displayed) |
The circuit breaker is in disconnected position. |
To check the details on the current Active alarm, refer to the submenu.